Could you tell me how to select the positioning operation or the pushing operation when entering the step data with PC to LECP6/LECA6?
When selecting the Normal mode or the Easy mode of setting software of LECP6/LECA6, the setup software returns the following error messages.∗ Normal modeThe COM port setting may be wrong!∗ Easy modeNo communication to the controller. Edit communication setting?
I could not turn the servo motor ON to operate an actuator when setting up LECP6/LECA6.
When using the LECP6 and LEFS units, are sensors required for the return to the origin?
When shutting off the power supply to the controller LECP6/LECA6 and then resupplying the power to the controller, is it necessary to perform the return of the origin?
According to the instruction manual of LECP6, the power is separated into the control power and motor power. Why are there two types?
How can I stop electric actuators with the controller LECA6?
I tried to change the direction of the return to origin with the controller LECP6, but the direction was not changed.
Regarding actuators with locks, is the 24VDC for releasing the lock required during normal operation by the LECA6/LECP6 controllers?
We started to test an LE∗ electrical actuator, but it doesn't function (strange movement) The driver is LECPA(pulse input type step motor driver).
We are setting the control side of LEC∗6 electrical actuator. We are working on setup with LEC-G(gateway unit), but communication is not possible. Can you please explain?
How can step data numbers be input from the PLC?
Is it possible to the return to origin operation repeatedly with LECP6/LECA6?
Is it possible to switch to the another step data operation during positioning operation without stopping when using In LECP6/LECA6 controllers?
Is it possible to change the return to origin direction for LECP1 controller?
Is it possible to switch to the next operation during positioning operation without stopping when using LECP1/LECP2 controller?
I cannot manually move the slide table of an actuator with a controller unconnected. Is there a way to do this?
In step motor type LE series, if the position of a slider such as the table is displaced with external force, will the set value of the next target position be also changed?
Can the controller configuration software (LEC-W2) be downloaded from the homepage?
Why is an alarm generated when commanding a "SETUP" request (return to origin) 1 second after SVON (servo on)?
Is it necessary to wire IN0 to IN3 inputs fully for the LECP1?
I have a controller setting software only. Can I connect the controller to my PC if using a commercially available connection cable?
What is the difference between "RESET" input and "STOP" to stop the actuator during normal operation?
Is it possible to detect the size of work pieces by pushing force mode of the LECP6? Is it all right to use INP output for this?
Is there a homing sensor built into the LE series?
What kind of processing is applied to the terminal of upper equipment (PLC side) of I/O cable (LEC-CN5-∗)?
Are there any actuator cables other than robot cables?
What kind of signal is 'SVRE' signal for LECA6/LECP6/LECPA?
Is a teaching box or controller setting kit required for LECA6/LECP6/LECPA?
Is it possible to operate LECA6/LECP6 so that it could be stopped during positioning operation of step 0 and then changed to execution of step 2?
What kind of signals do LECA6/LECP6 send out during positioning operation?
Arrival time abnormal' (1-149) is generated during thrust operation. What is the reason?
SVRE signal does not output from LECP6/LECA6 controller (Servo does not turn ON.)
When SVON signal is turned ON after applying power to the LECA6 controller, the actuator moved about 10mm. Why does it move?
What is the cable bending radius?
When the power supply is turned on again with the control power supply ON after returning to origin, is it necessary to return the actuator to origin again?
When the actuator is mounted vertically, will the table (rod) drop by its own weight?
Is it possible to rotate LER table physically by rotating the table?
We are going to change our actuators to those with a different size and stroke. Therefore, we also want to change the actuator applicable to the controller. Please tell us how to change.
Is there any problem if we want to mount LEF series actuator horizontally on the ceiling ?
When driving a step motor type actuator, will a dedicated controller be required?
I connected LECA6/LECP6 to PC using a controller setting kit but they don't become online. (Communication is not possible.)
Is it possible to switch LECA6/LECP6 actuators to a backward movement while they are moving forward?
What will happen if an electrical actuator is brought to an emergency stop during operation (EMG was put into a non-energised state)?
We purchase 'products with lock' because we use them vertically. How will the lock work when a product is bought to an emergency stop during operation (EMG was put into a non-energised state)?
How is the lock controlled in electric actuators with lock?
How does the electrical actuators thrust type return to origin work?
Please tell me the difference between positioning operation and thrust operation of electrical actuators.
What will happen if 'step no. IN∗' and 'DRIVE' are instructed at the same time in positioning operation?
What is thrust operation?
What is the difference between ABS (absolute) and INC (incremental) in 'operation method' in step data?
What is an area (output) signal?
How can I change the electrical actuator 's original point from the return end (motor side) to the starting one (Opposite to the motor side)?
How can I change the basic parameters after changing the electrical actuator's direction of return to origin? (Even if an address is specified, it doesn't operate and an alarm is generated.)
As the 〔ALM〕 on the controller turned on, I check the alarm description on PC (or teaching box). The position deviation counter indicated overflow 1-196 (or deviation overflow). What does this mean?
As the 〔ALM〕 on my controller turned on, I checked the alarm description on PC (or teaching box). It indicated 1-149 which means Failed to reach the target within set time. What does this mean?
As the 〔ALM〕 on my controller turned on, I checked the alarm description on PC (or teaching box). It indicated 1-192 (or encoder error). What does this mean?
As the 〔ALM〕 on my controller turned on, I checked the alarm description on PC (or teaching box).It indicated 1-193 which means phase detection was not possible within time (or magnetic pole undetermined). What does this mean?