Electric Actuators »
Download Controller Setting Software AC Servo Motor Driver(MECHATROLINK compliant)For LECYM/LECYU
Download Controller Setting Software
Decompress the downloaded file before use.
Install the software to the PC according to the Installation Manual.
▶Operation Manuals / Installation Manuals
Note: The Controller Setting Software (Chinese version) is a PC software that can only be used in a Chinese language environment. The software will not operate normally in PCs with language environments other than Chinese.
AC Servo Motor Driver(MECHATROLINK compliant)
For LECYM/LECYU
For LECYM/LECYU
Compatible Controllers | Name | ![]() |
---|---|---|
LECYM LECYU |
Setup software (For LECYM,LECYU) SigmaWin+ (ver.5) |
![]() |
LECYM LECYU |
Setup software (For LECYM,LECYU) SigmaWin+ (ver.7) |
![]() |
Compatible Controllers | Name | ![]() |
Note |
---|---|---|---|
LECSB2-T、LECSC2-T LECSS2-T、LECSN2-T |
AC Servo Motor Driver / (Parameters read from setup software (MR Configurator2™)) |
ー | Setup software can be arranged through the catalog options. Click here for catalog |